This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC8T245: Will the device work if powered up with DIR pulled to VCCA and OE pulled to GND?

Part Number: SN74LVC8T245
Other Parts Discussed in Thread: ASH

Question:  Will the part work if I power it up under the following conditions –

                DIR Pin: Pulled up to VCCa

                /OE Pin: Pulled low to GND

The spec says that it should be started with both /OE and DIR pulled-up to VCC, but I cannot spare an IO pin to control DIR or /OE, so I want to hard program them into the desired operating state (data flow from BusA to BusB).