This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1G125: Need to know maximum capacitive load driving capability

Part Number: SN74AUP1G125


I would like to know the maximum capacitive load that can be driven by SN74AUP1G125DCKR. I have seen in the datasheet, in the test conditions, that it can drive up to 30pF. The design in which we are using this part,it is required to drive up to 50pF. So the question is, can this part support 50pF load?

Thank You!