This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: Does TXB0108 have any diode for ESD protection at An, Bn and OE terminals?

Part Number: TXB0108

 Hello guys,

 One of my customers is considering using TXB0108 for their next products.

 They have the following questions about TXB0108. Could you please give me your answers or comments?

 Q1. Is there any ESD protection diode (parasitic diode included) from GND to A1~A8, B1~B8 and OE terminals?

 Q2. Is there any ESD protection diode (parasitic diode included) from A1~A8 to VCCA, from B1~B8 to VCCB and from OE to VCCA terminals?

 Q3, If the answer for Q2 is yes, is the diode still active when OE=GND? It seems that the diode is not active when OE=L because VI and VO absolute maximum rating is described as 6.5V and it does not depend on VCCA and VCCB voltage.

  Your reply would be much appreciated.

 Best regards,

 Kazuya Nakai.