Other Parts Discussed in Thread: SN74AVC4T245
The datasheet for the SN74AVC4T245-Q1 (page 19) states that to ensure the high-impedance state of the outputs during power up or down, the OE pin must be pulled high.
I DO NOT need to guarantee the outputs are high-impedance during power up, but I DO need to guarantee they will NOT be driven high.
For example, if the initial condition is:
* VCCA, 1DIR, and 2DIR are all stable at 3.3V
* 1OE, 2OE are tied to ground
* 1A1, 1A2, 2A1, 2A2 are all pulled low
* VCCB pulled low (VCCB un-powered and pulled low through a resistor)
If I then apply power to VCCB, I need to ensure the outputs will not be driven high at any point as VCCB ramps up.
Can you please comment on expected operation in this scenario?