Part Number: SN74GTL2003
Other Parts Discussed in Thread: TINA-TI
Hello,
My customer is using SN74GTL2003 to translate between 3.3V and 1.2V. The current design now needs to translate between 1.2V and 1.05V. The data sheet says that the the GREF input must be connected to DREF and both pins pulled to HIGH-side VCC through a pullup resistor (typically 200 kΩ). But the high side (1.2V) is now connected to the S inputs.
The current plan is to rotate the chip 180 degrees which will put the 1.2V signals on the D side and 1.05V signals on the S side. The only problem is the need to supply 1.05V to the SREF pin and 1.2V is only available. A resistor divider could be used to lower the voltage at SREF, but we don't know the input impedance of SREF pin to figure out what resistance would work. The customer is thinking of a resistance value that is low like around 100 ohms which would only dissipate about 12 mW.
Would this resistance value work in this fashion? Do we have the impedance information for the SREF pin?
Thank you so much for your help!
Best regards,
Errol Leon
Texas Instruments
Field Applicaitons Engineer