Part Number: SN74AVCA406L
Hello team,
I am considering level shifter for SD card and I have questions about SN74AVCA406L and TXS02612 below.
1) SN74AVCA406L's fmax spec of clock and data is described as 95MHz in its datasheet when VCCA=1.8V, VCCB=3.3V. Is this 95MHz data meaning 190Mbps?
If no and it means 95Mbps, does the device support DDR50?
For TXS02612, it specifies these in MHz for clock and Mbps for data.
2) SD card side supply(VCCB or VCCA) is start with +3.3V. However it needs to reduce to +1.8V during initialization sequence. Can these device accept VCCB or VCCA change during operation?
I am afraid if the condition may cause some issue.
3) Do we have voltage level shifter IC for SD that supports SDR104?
Best regards,