Part Number: SN74LS156
Other Parts Discussed in Thread: SN7400, , ULN2003A
this may sound stupid but my mind isn't working: Problem how many 14/15ma loads will this device tolerate with a 3.5vdc rail without buffering. the devices are both 16 segments (alphanumeric) and 7 segments. They are NOT LED but lamps and very expensive. In my mad hairbrained idea, I am using 27 74LS240 for the drive and using the gate control input a PCM signal used for device dimming. this will drive one segment. By using a group of 74LS156 with Open Collector Outputs and a 3.5 vdc as HIGH. So here goes when a segment is driven HIGH by the 240 out and it is not selected via a HIGH on the decoder, Nothing Happens (even with the 240 in TriSate mode). But if the decider is a LOW you will get current flow. So I have to sink somewhere between 30 ma for a 1 to 240ma for a 16segment Lamp test.
#2 where can I get a 3.5volt regulator