This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN54AC244-SP: Are the data and control inputs 5V compatible when this part is powered at 3.3V?

Part Number: SN54AC244-SP


It was not clear from the datasheet whether the data and control inputs can handle 5V inputs when VCC is 3.3V without damaging the part.  The absolute maximum ratings includes a Note 1 that says: "the input and output voltage ratings may be exceeded if the input and output current ratings are observed".   Which input/output current ratings does this refer to?  Note that I am interested specifically in the space-grade version of this part, since our application is for space.

Thanks very much,

Ted