Part Number: SN74LVC16T245
Other Parts Discussed in Thread: SN74LVCR16245A
Hello
i have a problem using SN74AHCT126DGVR,SN74LVC16T245DGVR
i have 2 types of discrete line:
1). configurable discrete which is connected to both SN74AHCT126DGVR (used as output driver),SN74LVC16T245DGVR(used as input buffer/voltage converter, both ICs are 5V (VCCB) and the control line/Fpga input is 3.3V(VCCA) . once the line is set to output ,the input buffer is 'Z' and the other way around
2). Output discrete which is driven by SN74LVC16T245DGVR, 5V (VCCB) 3.3V(VCCA)
when both configuration set to output , configuration 1 give me 7v on the output as "high" , and on configuration 2 i see normal levels. what is the reson for that? is it related to the different logic famelies(HCT and LVC)?
configuration 1:
configuration 2 :