This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G126: Rise- and fall-time, switching speed

Part Number: SN74LVC2G126


Hello,

i got a couple of questions regarding the device sheet.

  1. 6.3 Recommended Operating Conditions: Delta_t /Delta_v a the Input is 10ns/V
    1. Does this mean, that the Output can't follow the Input rising anymore?
  2. 9.2.3 Application Curve : Is this the frequency behaviour for single frequencies?
    1. Because when I got a 40 MHz digital Signal, then 100 MHz wouldn't be enough for the switching Speed I suppose

Hopefully I explained it well enough=)

Kind regards, Manuel