Part Number: TXS0104E-Q1
Hi Team,
I would like to verify the OE spec in the datasheet. I see that the maximum voltage level for OE is 5.5V. I was surprised to see that this maximum is not referenced to either one of the VCCs. Is that accurate?
Is it acceptable to use 5V on the OE pin in the scenario where both VCCs are at lower voltages (for example VCCA = 1.8V and VCCB = 3.3V)?
Thank you for your support,
Jared