Other Parts Discussed in Thread: CC1101
Hello!
The converter does not work. At the output of 1.6V.
When transferring data, there is no conversion and the signal is very strange.
What is the problem? Conversion should be 3.3-5V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am going to need a better schematic. What frequency are you operating at? Are you using any external pullups on the device?
Here is an appnote on translating with TXB: cdn-shop.adafruit.com/.../txb0108appnote.pdf
Thanks!
-Karan
Hello!
1. Frequency about 1 MHz
2. A microcontroller (ATmega328) is connected to the converter. External and internal (pullups and pulldowns) are not, MCU side connect:
- CSn connect to PB2 (OC1A/PCINT1)
- GDO2 connect to PD3 (PCINT19/OC2B/INT1)
- SO connect to PB4 (MISO/PCINT4)
- SCK connect to PB5 (SCK/PCINT5)
- SI connect to PB3 (OC2A/MOSI/PCINT3)
I use hardware SPI for CC1101
It all worked. The reason was that during installation the PCB was bad washed.
The flux was under the chip.