Part Number: TXB0108
Other Parts Discussed in Thread: TPS3808, SN74AUP1G34
Hello,
Our customer asked to keep the level shifter disabled while the system is in reset, mainly to ensure no leak during power-up.
Can I connect an open-drain output (pulled to 1.8V) of a system-reset generator (e.g. TPS3808) to the TXB0108 ENABLE pin?
Or that there is a need to have a pull-down as is specified in the spec.
If there's a need to have a pull-down - how can I enable the level shifter when power is on?
Here's my schematic. For clarity, removed the I/O signals.