I would like to know if having a pullup on the output of the SN74ABT827 creates any issues with the specifications.
The VCC is +5V and the pullup is 10K to VCC.
Normally Cmos outputs do not like to have pullup or down resistors.
This part does not have a high side output diode to the VCC rail. It only has a low side diode to GND.
Hence the caveat is in the specifications and it appears that adding a pullup to VCC can potentially inject current into the output pin which generally is not accepted without high side diode.
Are there issue with this pullup on the output?