I'm looking for a solution to translate between 3.3V and 5.85V. Outside of old CD4K type devices that are too slow, I was thinking about using a TXB or TXS type device. The driving logic is push-pull, so I'm leaning towards TXB. These translators are typically spec'd to have VCCB up to 5.5V , but the Absolute Max rating is 6.5V.
Are there concerns about operating these translators with VCCB = 5.85V?