This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1G17: About output level at Vcc<0.8V and Input =2.55V-3.4V

Part Number: SN74AUP1G17


Hello,

 

Regarding to output on SN74AUP1G17, my customer is asking a question. 

(Question)

When their conditions are as following, how does output level become?

(High or low or unknown?)

・Vcc<0.8V (under 0.8V)

・Input A =2.55V-3.4V

 

Basically, I think that the device is not damaged at input 3.4V, because of Absolute Maximum Ratings.

But I’m not sure how output level become on above conditions.

 

Regards,

Tao_2199