Part Number: LSF0108
Hi Team ,
My AA large customer is in a progressive layout phase right now with the LSF0108.
The design team wishes to control the EN pin dynamically by setting it to GND using a pull
down resistor and while they need to use it they will enable it.
The application notes , D/S and EVM are always showing
a 200K PU to the higher voltage rail (Rail B).
1. Can they use this EN pin dynamically ?
2. Do they need the PU at all if they are driving this pin from another source when
it is required ? (any special voltage limits required or slew rate or else)
3. What should be the typical PD resistor if the above use case is OK ?
Please advise urgently ,
Arik.P.