Other Parts Discussed in Thread: SN74LVCH244A
Hello, in a massive product PCBA, we found some error when we used SN74LVC244APW to replaced SN74LVC244ADB (we used one compliant PCB pads to both 2 package).
We do the trouble-shooting and found there is a hardware design bug that the output have NO pull-down resistors, so when the /EN is high voltage level the output is sensitive to noise.
But we found that if we change SN74LVC244APW back to SN74LVC244ADB, then it can become OK.
We would like to ask:
1. whether SN74LVC244APW and SN74LVC244ADB have different chip die? or manufacture batch? cause thie difference.
2. If there is any pin-to-pin package chip to replace the SN74LVC244, which do not have high-impedance output(for example-bus hold) characteristics when /EN is high voltage level.