Part Number: TXS0108E
Other Parts Discussed in Thread: SN74AVC4T774, SN74LVC1T45
Hi Team,
I plan to use the TXS0108E in my EVM board to transfer the voltage level between MCU controller and the device IC.
Here i have 3 questions,
1. i will not control the OE pin, should i connect it to VCCA or GND? I am confused by the related description in the datasheet. From my understanding the I/O pins should be in Tri-state output-mode.
2. This IC can be used in UART communication case?
3. Does this IC support constant level transfer? For example, constant 3.3V (high) input transferred to constant 5V (high) output.
Thanks and best regards,
Felix