Other Parts Discussed in Thread: LMH6881, , SN74LVC1G14, SN74LVC2G14, SN74LVC3G14
Hi team,
Need to level shift a 0V logic 0 reference to -1.25V logic 0 reference for the LMH6881 device SPI working with max 50MHz SCLK frequency. Could you suggest a suitable part number for the same which can do it? Is SN74LV4T125 the right logic level translator?
Best Regards,
Rohit