Part Number: TXS0102
Hi,
can we add an external pullup in parallel with the on-device 10K to run faster than 2 Mbps? What dictates the 500 ns pulse duration spec'd? Isn't this primarily a factor of the external capacitance present at the device input or is this some how related to the One-shot accelerator in the device? Along the same line, why is this spec so dramatically improved by using a push-pull driver?
Thanks,
Sal