Part Number: CD74HCT7046A
We are now using HCT7046 for FM demodulator design, the sch is same as datasheet FIGURE 1. LOGIC DIAGRAM as below, R3=3.3k, C2=470pF. signal frequency(intermediate frequency) applied on pin14 is 10.7MHz, 280kHz bandwidth, power supply is 5VDC.
LD signal on pin1 is always high so PLL is locked well, power supply noise is very small, and the 10.7MHz signal is very stable, the converting function between input frequency(on pin14) and output DC voltage(on pin10) is good. but the signal on Demo_out pin10 has noise with frequency between 12kHz to 70kHz and with amplitude of 40mVpp. We have taken many trials to remove this noise or try to move this noise to high frequency for LPF easily remove, but the noise is very very hard to change.
This noise frequency range is overlaped in signal band, so my question is if this noise is normal component in the Demo_out signal? how to remove this noise? or if this noise can't be removed how to move the noise frequency to higher end up to several hundred kHz for easily LPF kill?
Thanks!