Other Parts Discussed in Thread: LSF0102
Hi,
In our application we need translation between 1.2V and 1.8V. Can LSF0102QDCU-Q1 use as level translator in this case? Because in datasheet it is mentioned that " Vref_B should be in the range of Vref_A + 0.8 to 5.5V. Also Vref_B and VI(EN) are recommended to be at 1.0 V higher than Vref_A for best signal integrity. So is it make a problem if i use this part for translation between 1.2V and 1.8V ?