Part Number: SN74AUP1G126
Hi guys,
Question from a customer:
The data sheet states OE pin disables the input pin of the buffer. I have a question based on the statement of the input being disabled when OE pin =GND.
If VCC pin = 0V, Gnd pin=0V, OE pin=0V, input pin=3.3V, will it damage the buffer IC?
I’m looking at using this in a battery powered device, there are cases that last for about 1-2 sec when the buffer VCC=0V, Gnd=0V, OE=0V, and Input=~3V. After the 1-2seconds the buffer will have VCC=3.3V, OE=3.3V, GND=0V, input=~3V.
If the input is actually disabled with OE pin, then applying a voltage to the input won’t damage or latch up the part.
Thanks,
Brian