This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: TXB0104QPWRQ1 level translator is failing to translate from low to high & high to low when processor gpio pin is set to out(in/out),can you please help to resolve the issue.

Part Number: TXB0108


TXB0104QPWRQ1 level translator is failing to translate from low to high & vice versa when processor gpio pin is set to out(in/out),can you please help to resolve the issue.

 

Issue explained below:

 

When processor is set to out and gpio pin will be at high level(1.8V) which connects A side of level translator(VCCA=1.8V) and when low is passed from 3.3V devices through B side level translator(3.3V) its observed that the processor GPIO pin is still at high & failing to pull down to low by level translator, please help to resolve the issue.  

 

Thanks & Regards,

Satish