Hello,
how does the SN74LVC1G14 behavior in case of VCC=0V and Vin=3.3V? Is this allowed?
Customer needes the min/max values for ∆VT Hysterese (VT+ - VT-) Vcc=3.3V (datasheet page 6, chapter 6.5). Can you give me the values.
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
how does the SN74LVC1G14 behavior in case of VCC=0V and Vin=3.3V? Is this allowed?
Customer needes the min/max values for ∆VT Hysterese (VT+ - VT-) Vcc=3.3V (datasheet page 6, chapter 6.5). Can you give me the values.
Regards, Holger
Hello,
The case of VCC = 0V and Vin = 3.3V is defined in the electrical characteristics table:
The input and output are in high-impedance if the supply is 0V. The input can be up to 5.5V.
For ∆VT Hysteresis (VT+ - VT-) at 3.3V, I would recommend determining this value at the supply limits for the customer. For example, if their supply has a 5% tolerance, you can use linear interpolation to find the values as shown here:
Then the worse case for each spec should be listed. For example, VT+(max) is the worst at +5%, so teh value of 2.1397 would be used.
Here's the linear interpolation file I created for this: