This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] What does 'partial power down' or 'Ioff' mean in the datasheet?



FAQ: Logic and Voltage Translation > Logic Technology >> Current FAQ

The "Ioff" specification in the electrical characteristics table is only in the datasheet of devices that have the special feature of "partial power down" - also known as "back-drive protection."

Partial power down protection is the lowest level of live-insertion isolation, as defined by the application report "Logic in Live-Insertion Applications."

Partial power down essentially states that, if the supply of a device is held at 0V (any supply for multi-supply devices), then the input and output pins of said device will enter a high impedance state. The maximum leakage current in this high-impedance state is defined by the Ioff specification in the datasheet.