This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SVID Redriver



Dear Team,

My customer is using Intel core chip and DC/DC controller with SVID protocol.

But the layout between Intel and DC/DC controller is too long, do we have suitable redriver here?

SVID is a low voltage (1.0V) serialized bus running at ~ 26MHz according to the online specification. 

Nasser Mohammadi mentioned:

Our signal conditioning devices are meant to operate for a much higher data rates – 100MHz and higher data rates. At 26MHz, there is not much loss and our signal conditioning devices do not boost this signal. Also, please note our signal conditioning devices are used with NRZ type of data. SVID uses mainly CMOS or TTL level logic.

BR

Kevin