Part Number: CD4013B
I am using CD4013B D-FF for Latching purpose.
Here Clock is fixed to Vcc and D input also fixed.
1: Need to know the valid status of Q when Both SET and RESET are low and (Data and Clock are Don't care).This state is not mentioned in datasheet.
2: Do you have any alternative for CD4013 D-Flip Flop with same function table but with higher output driving current and AEC Qualified.
Here it is only 360Ua. Needs current rating around 10mA.
3:Also require its Junction temperature(Not mentioned in Datasheet)
4:Please can you provide me the PSpice model for CD4013B D-FF.
As per simulation it is showing 0.5*Vcc or half of Vcc.
5:If possible please provide me the application note for the same.
with regards,
Siddharth Sangam