This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHC245: what is the input impedance of SN74AHC245QPWR

Part Number: SN74AHC245


What is the input impedance of SN74AHC245QPWR?  When I put an RC filter(100ohm+1nF) at the input. The high level and low level of input signal are 5V and 0V. But i can only see 4.1V after the resistor. So i am wondering if it is ok to add an RC filter at the input pin.

Regards,

Yangbo