Part Number: SN74LVC1404
Other Parts Discussed in Thread: SN74AUP1T50
Hi all,
Below is the schamtic, when all three outputs are used, high level volatage of OSCIN_24MHz is 1.27V , AEC_24MHZ is 1.2V,HDMI_I2S2_MCLK is 0.65V, (clock high level minimum 2.31V) . The voltage is too low. But when I delete one output, the left two outputs are :OSCIN_24MHz -2.89V , AEC_24MHz -3.05V ,which meet the requirement.
1. Does this chip not support three outputs because of output current?
2. If I want to support 3 outputs, can I use a buffer like SN74AUP1T50 to buffer one output, as two outputs are OK, or do we have socket can support 3 outputs?