Part Number: TXS0101
I am using TXS0101 as a level translator between two serial I/O pins. They are 3V to 5V, open-drain, data rate less than 10 kbps. 16 bytes of data were input to the A port but only two bytes were seen in B port. OE is enabled and by-pass caps are 100 nF each. What could be the problem here?
Here are the signals from the input and output pins: