This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVCB3T16211 availability and alternate part

Other Parts Discussed in Thread: SN74CB3T16211, SN74ALVC164245

Hi,

I am trying to use the SN74LVCB3T16211ZQLR part for the prototypes and these are becoming very difficult to buy.

I have been trying to order them from Sept 2010 and since then they are shown as being back-ordered.

Is there any other distributor other than Rochester Electronics that can sell this part in lesser quantities (Rochester

sells them only in higher quantities).

 

Also, is there another part which has the same features as SN74LVCB3T16211ZQLR (converts 5V inputs down to

3.3V) ? If so, can I have the part number. Also, one more thing, the part should be as small as the above (no bigger than).

 

Thanks,

Regards,

Aditi.

 

  • I'm sorry for the delay.

    Are you refering to the SN74CB3T16211? it looks like they are currently available from both digikey and newark. 

    An alternate suggest would depend on your application and max frequency. The SN74ALVC164245 is one option.