Part Number: TXS0102
Hello,
I am using the TXS0102 level-shifter between a 4.5 V (VCCB) and 2.5 V (VCCA).
On of the 2 signals is coming from a NAND gate to a MCU; and this signal works.
The second one is coming from a comparator (to the same MCU) and its voltage is at 0.5 V (more or less) even when the comparator output should be 0.
When disconnecting the level-shifter, comparator output is well at 0V and global consumption drops.
I though a pull down will help but even with 1k, the signal drops to 0.3V like something inside pull-up the signal and increase the consumption.
Can you explain this ?
If the chip is broken, could it be because VCCB is before the enable and VCCA ?
Looking forward to your feedback!
Best regards,
Sarah