This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Data request on package MF03A (LM4041)

I'm working with an LM4041AIM3-1.2 (formerly a National Semi part), in package MF03A.

Looking at the package drawing on the datasheet, the "Gage Plane" looks like it is located between the 2 bends in the leads.  I'm trying to determine the maximum lead height.

If the Gage Plane (at 0.008") is indeed between the 2 bends, and their inside is 0.004" radius, and the leads are 0.005" thick, that puts the max lead height around 0.018".  If I just figure the Gage Plane

is halfway up the leads, then the max lead height is about 0.016".  I just need to verify that the max lead height is less than 0.031", and this looks like a pretty safe margin, unless there's a straight

section between the 2 bends that isn't shown on the drawing.  Can you tell me if my estimates are good, or if there is a straight section that's not on the drawing?

Thank you.