Part Number: SN74HC541
Other Parts Discussed in Thread: CD74FCT541
Hi
Our customer are looking for the buffer of high output current. The output current (ABS) of this device is 35mA. They want more than 30mA or 40mA of output current. (Also Icc is more 120mA)
They need OE function also.(no 3 state output. They wan L output when the input is Hi-z.)
Do you have any device that the above requirement is met?
I think the open collector type of the buffer is met to the requirement. But the output may be high when the input is Hi-z.
Best Regards,
Koji Hamamoto