This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dual low-side switch with adjustable break-before-make time

Other Parts Discussed in Thread: DRV103

Dear TI-Team,

we're looking for a switch to control to dry contacts of an external motor relay (UP and DOWN). It is important that there is at least one second of delay when the MCU toggles the direction while the motor is running and I don't want to leave it only to the MCU. Is there an IC which can be used for this? System voltage is 24V, MCU's logic voltage is 3.3V