Part Number: SN74LVC157A
Other Parts Discussed in Thread: SN74AXC1T45
Hi all
Would you mind if we ask SN74LVC157A?
There is the description "Maximum Output rating VCC+0.5V" on the datasheet.
Does "this 0.5V" mean protection diode between output and VCC?
How much is the maximum current for this diode?
As the background of this question, our customer would like to use this device as follow conditions.
-Vcc=2.5V
-there is the pull up with 3.3V
->In this case, output is more than absolute maximum rating. So, we would like to confirm whether "VCC+0.5V" is due to protection diode or not.
Kind regards,
Hirotaka Matsumoto