Part Number: SN74AVC16T245
Hi, staff
I have a question about the level shifter.
Questions concerning the power sequencing in the datasheet of the level-shifter of 1. to 10. below.
There are devices with power sequence comments in the data sheet and devices without comments.
Since they are all the same AVC series, are the power-on sequence all the same?
For a device that does not have a description of the power-up sequence in the data sheet,
is it safe to start Vcca or Vccb first?
(There is no power-up sequence)
The data sheet was compared whether there is description of the power-up sequence or not.
1. SN74AVC16T245DGVR :Not described
2. SN74AVC1T45DBVR :Stated Yes Vcca -> Vccb
3. SN74AVC2T45DCUR :Stated Yes Yes Vcca -> Vccb
4. SN74AVC4T245PWR :Not described
5. SN74AVC8T245PWR :Not described
6. SN74AVCH16T245VR :Not described
7. SN74AVCH4T245PWR :Not described
8. SN74AVCH8T245PWR :Not described
9. SN74LVC1T45DBVR :Not described
10. SN74LVC2T45DCU :Stated Yes Vcca -> Vccb
Is it correct with the understanding that the above-mentioned level shifters are not regulated by Vcca and Vccb in magnitude of voltage?
(It can be used even if Vcca> Vccb, Vcca <Vccb)
best regards
cafain