Other Parts Discussed in Thread: SN75155
Have the same Issue with OUTSEL set to H
VCC1 and VCC2 are 5V
OUTSEL set to H = +5V
INV RESET set to H = +5V
Inv OE set to L = 0V
Have serveral SN74LV8153 in an Isolation Application to set Multiplexer Adress Lines. This did not work.
Figured out that Outputs are only high connecting a Pull-Up Resistor to VCC.
The Devices are not in OC-Mode, checked Logic Levels: They are not inverted.
Got all chips 2 weeks ago from digi-key.