Part Number: SN74HC244
Hello Team,
Looking to the SN74HC244 datasheet I do see that the absolute max Tj is 150C while the recommended operative temperature (ambient) is 85C.
I f the device is not loaded working at low frequency (2.5KHz at 3.3V and Iload <1mA).
The T increase from ambient should be low.
- Would be possible to operate the SN74HC244 at 105C ambient?
- Do you have alternatives to the SN74HC244 that may operate at 105C and integrate ESD diodes?
Thanks
SunSet