This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVCA406L: SN74AVCA406L

Part Number: SN74AVCA406L

TIサポートセンターご担当者様

いつもお世話になっております。川上と申します。

上記ICにて、技術的なご質問がございます。

一時的に、電源電圧をVCCA:3.3V、VCCB:0Vにし、B側のピン全てをハイインピーダンスにするな使用を考えております。
このとき、A側のピンをDIR設定で出力に設定した場合、何が出力されるのでしょうか?
We are planning to temporarily set the power supply voltage to VCCA: 3.3 V, VCCB: 0 V, and make all the pins on B side high impedance.
At this time, what is output when the A-side pin is set to output with DIR setting?

ex)
VCCA:3.3V
VCCB:0V
CMD-dir:L (CMDB to CMDA)

⇒CMDA:? (H,L or Hi-Z ?)

データシート上には、下記の記載しか無いようですが詳細の情報があれば頂きたいです。
Although it seems that there is only the following description on the data sheet, I would like if there is detailed information.

【If either VCC is switched off (VCCA = 0 V and/or VCCB = 0 V), all outputs are placed in the high-impedance state to conserve power.】

以上です。よろしくお願いいたします。

Best regards,