Part Number: CD4041UB
Hi ,
I want to use CD4041UBPWR ,it is new componnent for me , can you PLS tell my about the relability of the CD4041UBPWR?
Thank you.
Ilan mazuz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CD4041UB
Hi ,
I want to use CD4041UBPWR ,it is new componnent for me , can you PLS tell my about the relability of the CD4041UBPWR?
Thank you.
Ilan mazuz
Hi,
in order to gate more current can i shorts the inputs to the input signal ,then short the outputs to the output signal?
BR,
Ilan
12-14mA sink and source with 10v high and 0.5v low.
20mA sink and source.
PLS answer for my question before.
I mean shorting inputs and outpts.
Thanks
Ilan
Hi Emerys,
How much current sink and source is 100mW per channel when VDD=10V at output?
How the current at output is sharing between the channels I was connected together?
Thanks
Ilan MAzuz