Part Number: TXB0106
Other Parts Discussed in Thread: SN74LVC8T245, SN74LVC1T45, SN74LV4T125, SN74LV1T34
Hello Support Team
I have a need for a 6 - bit high speed bidirectional voltage translator. On one side, I have a CPU powered with 3.3 V, and on the other side is a target device with adjustable power 3.3V or 5V. I tried using TXB0106 but there is a signal distortion. Please see attached pictures, CPU on A side of translator is sending a 500 kHz signal, on both sides VCC is 3.3V, C1 is A1 pin and C2 is B1 pin of TXB0106, PIC1 are signals without target connected (looks good) and PIC2 are signals with target connected (there is a distortion in signal on B side). Can you tell me what is causing signal distortion?
Can you please recommend some of your other devices suitable for this kind of a design? There can not be any pull-up on the data lines, possible pull-down resistors.
Thank you,
Kind regards,
Nenad Jovanovic