Part Number: TXB0108
Hi TI community,
I'm working with a design that uses the TXDB0108 to step up 3.3V lines coming from a Spartan-6 FPGA to 5V.
The pin-out is simple... with the GND pin grounded, and connected through a (56k) resistor to the OE pin. VCCA (toward the FPGA) is 3.3V, while VCCB is on a 5V rail. Finally, there are additional pull-up resistor on each of the logic lines coming out of the 5V side.
The logic lines from the FPGA are 3.3V CMOS. I'm able to apply these signals successfully to one side of the chip, but the corresponding line on the 5V side remains at 0V.
I know there are requirements for driving pins on the TXDB0108, so I'm wondering if I need to change someone about the logic lines coming from the FPGA.
Thanks a lot for your help,
Ian