Part Number: SN74LVC8T245
Hi Ti,
my design is to make driver for optocoupler base on IC PNPS8101* with series resistance of 250 ohm to the LED.
I need to use output type push and pull, current sink and source output +/-12-14mA.
PLS tell me if one of the output is shorted to GND does the IC PN 74LVC8T245 will damage?
What is the different between current short output (IOS ) and maximum output current ( IO max)?
How can i protect the output from short to ground when i can not add another series resistance close to the output?
Thanks
Ilan