Part Number: CD4041UB
Hi Ti,
PLS advise if can i drive with IC PN CD4041UBPW (VDD=10v) the optocoupler PN PS8101 at temperature range from -40C to 85C ?
1.when i have 277 ohm near to output driver in series connect to another series resistance of 250 then the last connect to LED optocoupler.
2.When i use one input and output (one buffer from the 6 buffer) and the VOH=9V and VOL=0.5v.
Thank you.
Ilan