This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108-Q1: Operation when EN pin short to Vpu(=5V)

Part Number: LSF0108-Q1


Hello

we have some questions , could you tell us about below?

1:

according to the datasheet "9.2.1.2.1" , it described "the EN input must be connected to Vref_B and both pins pulled to HIGH side Vpu through a pull-up resistor
(typically 200 kΩ)."

   if Pull-up resistor is shorted and EN pin connected to Vpu(=5V) directly, in this case, are there any concerns?

   for example, device damag or uncorrect operation..

2:

How should we handle the unused terminals?
Can I leave open?

Best regards

Yamane