Part Number: TXB0304
Other Parts Discussed in Thread: TXB0302, TXB0106, LSF0108
I'm thinking of using TXB0304 plus TXB0302 to translate QSPI signals (clock plus DQ0...DQ3) from 1V5 (host, an FPGA) to 3V3 (could be 2V5 or 1V8 if that helps)
Datasheet mentions some maximum data rates but I think that's for individual signals. Synchronous data are affected by the delay difference that happens to be significant and I suppose it adds up to each signal degradation. On top of that I will be using more than one device as I have 5 signals and I'm concerned about the device to device variation as well.
How reliable is it to use those devices for QSPI? Ideally I'd be running them at >100 MHz but it can be acceptable at 50, even 40 MHz