Part Number: SN74LV1T08
Other Parts Discussed in Thread: 2N7001T
I am looking to use a SN74LV1T08 as a voltage translator between 1.8 V on the input and 3.3 V on the output. It is likely that at some point the input signals will be active while the output voltage domain is off. Will there be a load on the input if they are driven high into the part while its power is off?